NNZ6555700-01

Menu Bar

The Menu bar is displayed on the top of the screen and it contains buttons to access all the available menus as shown in the following image.

A

Menu buttons

B

Control panel status LED

C

Logout button

The Logout button is used to close the session.

The control panel status LED blinks in green when the control panel is active and in red when there is a communication failure with the DSP board.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?