NNZ6555700-01

Control Panel

The user interacts with the unit through the control panel located on the front panel of the PowerLogic™ DVR unit.

The control panel provides the information of the current operating status, instantaneous and accumulated values, and the possible events that causes the system to malfunction. The control panel is also used to edit some of the parameters.

The control panel screen is divided into three sections as shown below.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?