DOCA0257EN-00

Anti-Backspin Timer

Description

Anti-Backspin timer is used to wait until the motor is mechanically stopped.

Once the motor is stopped (electrically), this function keeps the LTMT main unit in inhibit mode until the predefined time delay has elapsed.

Parameter Setting

The anti-backspin timer function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Enable

Disable

Time Delay

0–60000 s in step of 1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?