DOCA0257EN-00

Phase Over Voltage

Description

The phase over voltage protection function generates the following signals:

  • Alarm: Any of the line-to-line voltage goes above the alarm level.

  • Trip: Any of the line-to-line voltage goes above the pickup level for the specified time delay.

Parameter Setting

The phase over voltage protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm

  • Trip

  • Alarm + Trip

Trip

Pickup

101–130% of nominal voltage in step of 1%

110% of nominal voltage

Time Delay

0.1–6000.0 s in step of 0.1 s

5 s

Alarm Level

101–130% of nominal voltage in step of 1%

110% of nominal voltage

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?