Device internal protection
Parameters Settings
The device internal protection function has the following configurable settings:
Parameter |
Setting range |
Default Value |
---|---|---|
Time Delay |
0.1–6000.00 s in step of 0.01 s |
1 s |
Reset Mode |
|
DI + Reset Key |
Internal Temperature Alarm |
|
Enable |