DOCA0257EN-00

Voltage Dip Management

Overview

When a voltage dip is detected, the LTMT main unit can perform two different functions to shed and reconnect the load automatically.

Selection is done through the voltage dip mode parameter:

If Voltage Dip Mode is

Then

None

Voltage dip functions are disabled

Load Shedding

Load shedding function is enabled

Auto Restart

Auto Restart function is enabled

Load Shedding and Auto Restart functions exclude each other.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?