Digital Outputs
![]() |
---|
UNINTENDED MACHINE OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The TeSys Tera system supports maximum of 13 digital outputs:
-
Three digital outputs on LTMT main units.
-
Up to 10 digital outputs with LTMT expansion units.
Output Configuration
The configuration of the digital outputs can be made through one of the following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.
-
The LTMTCUF control operator unit.
-
A PLC or DCS through the communication network.
Each digital output has the following parameters:
Parameter |
Setting range |
---|---|
Active type |
|
Output type |
|
Pulse time |
0 to 60000 ms in step of 1 ms |
Input source |
See list in input source |
The digital outputs are set by default depending on the motor starter type selected.
Output Type
The Active type, Output type, and Pulse time (t) parameters defines how the output information (A) is processed by the LTMT main unit and is converted in the physical information transmitted by the relay output (B).
DO Input Source
The most used input sources are indicated in the following table:
Index |
Input source |
---|---|
232 |
Pickup status |
233 |
Alarm status |
234 |
Trip status |
235 |
Motor stop error detection |
504 |
CONTACTOR OUTPUT 1 |
505 |
CONTACTOR OUTPUT 2 |
506 |
CONTACTOR OUTPUT 3 |
507 |
CONTACTOR OUTPUT 4 |
508 |
CONTACTOR OUTPUT 5 |
Refer to Input Source in Appendices for the complete list of input source.