DOCA0257EN-00

Maximum Number of Starts

Description

The maximum number of starts function helps to prevents the damage to the motor from frequent starts. This function allows the motor to start only for a pre-specified number within a given period of time. If the number of starts exceeds the set value, then this function keeps the LTMT main unit in inhibit mode, which helps to prevent any further motor start.

Parameter Setting

The maximum number of starts function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Enable

Enable

Permissive Starts

1–30 in step of 1

6 starts

Reference Time

15–60 m in step of 1

30 m

Inhibit Period

1–120 m in step of 1

5 m

Time between Starts

0–120 m in step of 1

0 m

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?