Components of TeSys Tera System
The hardware components of the TeSys Tera system are:
-
LTMT main unit
- LTMTCT/LTMTCTV sensor module
- LTMT expansion unit
- LTMTCUF control operator unit
The microprocessor based LTMT main unit is the central component in the system that manages the control, protection, and monitoring functions of three-phase and single-phase AC induction motors.
The LTMT main unit is designed to work with the following protocols:
- Modbus RTU
-
PROFIBUS DP
The system can be configured and controlled by using following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.
-
The LTMTCUF control operator unit
-
A PLC or DCS connected to the system through the communication network.
LTMT Main Unit
LTMT main unit |
Features |
Communication |
Reference |
---|---|---|---|
Modbus RTU
|
|
Modbus RTU
|
|
PROFIBUS DP
|
PROFIBUS DP
|
|
LTMTCT/LTMTCTV Horizontal Sensor Module
The following table introduces the key features of the LTMTCT/LTMTCTV sensor modules for horizontal mounting:
Sensor module |
Features |
Current range |
Voltage range |
Reference |
---|---|---|---|---|
LTMTCT modules with current transformers
|
|
0.3–3 A |
- |
LTMTCT3T |
2.5–25 A |
- |
LTMTCT25T |
||
10–100 A |
- |
LTMTCT100T |
||
LTMTCTV modules with current and voltage transformers
|
|
0.3–3 A |
60–690 Vac |
LTMTCTV3T |
2.5–25 A |
60–690 Vac |
LTMTCTV25T |
||
10–100 A |
60–690 Vac |
LTMTCTV100T |
LTMTCTV Horizontal Sensor Module for UL and NEMA Applications
The following table introduces the key features of LTMTCTV horizontal sensor module for UL and NEMA applications:
Sensor module |
Features |
Current range |
Voltage range |
Reference |
---|---|---|---|---|
LTMTCTV modules with current and voltage transformers |
|
0.3–3 A |
60–600 Vac |
LTMTCTV3UT |
2.5–25 A |
60–600 Vac |
LTMTCTV25UT |
||
10–100 A |
60–600 Vac |
LTMTCTV100UT |
LTMT Expansion Unit
The following table introduces the key features of the LTMT expansion unit. The maximum number of each LTMT expansion unit that can be connected to one LTMT main unit is also provided in the table.
LTMTCUF Control Operator Unit
The LTMTCUF control operator unit is the local Human Machine Interface (HMI) of the TeSys Tera system.
TeSys Tera DTM
TeSys Tera Device Type Manager (DTM) is a software module hosted in a Field Device Tool (FDT) container that uses the open FDT/DTM technology. For example, SoMove software.
In SoMove software, a specific DTM exists for the TeSys Tera system. The TeSys Tera DTM Library must be installed after installing the SoMove software.
SoMove Software
SoMove software is a Microsoft Windows-based application, using the open FDT/DTM technology.
SoMove software contains DTMs for different devices. The TeSys Tera DTM is a specific DTM that enables the configuration, monitoring, control, and customization of the control functions of the TeSys Tera system.
Cables
The components of the system require cables to connect to other components and to the communication network.
Connect to |
Cable |
Description |
Reference |
---|---|---|---|
LTMTCT/LTMTCTV sensor module |
LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.15 m (5.9 in) in length. |
LTMT9RJ1015 |
|
LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.5 m (19.6 in) in length. |
LTMT9RJ105 |
||
LTMT main unit to LTMTCT/LTMTCTV sensor module RJ11 connector cable 0.2 m (7.87 in) in length |
LTMT9RJ102 |
||
LTMT expansion unit |
LTMT main unit to LTMT expansion unit RJ45 connector cable 0.1 m (3.9 in) in length. |
LTMT9RJ401 |
|
LTMT main unit to LTMT expansion unit RJ45 connector cable 1 m (39.37 in) in length |
LTMT9EX10 |
||
LTMTCUF control operator unit |
LTMT main unit to LTMTCUF control operator unit connection cable 1.0 m (39.3 in) in length. |
LTMT9CU10S |
|
LTMT main unit to LTMTCUF control operator unit connection cable 3.0 m (118.1 in) in length. |
LTMT9CU30S |
||
PC |
PC to LTMT main unit or LTMTCUF control operator unit cable 2.5 m (98.4 in) in length. |
– |
|
Modbus network |
Modbus network communication cable 0.3 m (11.81 in.) in length. |
– |
|
Modbus network communication cable 1.0 m (39.3 in) in length. |
– |
||
Modbus network communication cable 3.0 m (118.1 in) in length. |
– |
||
PROFIBUS DP network |
PROFIBUS DP network communication cable 100 m (328.08 ft) in length. |
TSXPBSCA100 |
|
PROFIBUS DP network communication cable 400 m (1,312.33 ft) in length. |
TSXPBSCA400 |