DOCA0257EN-00

Average Voltage

Description

The LTMT main unit calculates average voltage and provides the value in Volts. The average voltage function returns the RMS value of the average voltage.

The LTMT main unit calculates average voltage using the measured line-to-line voltages.

The average voltage of three-phase motor is calculated using the formula:

Characteristics

Characteristic

Value

Unit

Volts (V)

Resolution

0.1 V

Refresh Interval

20 ms

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?