Current Phase Loss
Description
The current phase loss protection function generates the following signals:
-
Alarm: Any of the three-phase currents of the motor goes below 10% of the motor full load current.
-
Trip: Any of the three-phase currents of the motor goes below 10% of the motor full load current for the specified time delay.
-
Current phase loss protection function is not applicable in single-phase mode.
-
Current values that are less than 10% of FLC are considered as stop, and no value is displayed in metering and trip logs.
Parameter Setting
The current phase loss protection function has the following configurable settings:
Parameter |
Setting range |
Default value |
---|---|---|
Function |
|
Trip |
Time Delay |
0.1–6000.0 s in step of 0.1 s |
0.1 s |
Reset Mode |
|
DI + Reset Key |
Auto-Reset Delay (applicable only if Reset mode is Auto) |
0.0–6000.0 s in step of 0.1 s |
0 s |