Current Imbalance
Description
The current imbalance function measures the maximum percentage of deviation between the average current and the individual phase currents.
The current imbalance measurement is based on imbalance ratio calculated from the following formulas:
Calculated measurement |
Formula |
---|---|
If Iavg ≥ IFLC |
|
If Iavg ≤ IFLC |
|
Where
|
Characteristics
The current imbalance function has the following characteristics:
Characteristic |
Value |
|
---|---|---|
Unit |
% |
|
Resolution |
1% |
|
Refresh interval |
100 ms |