Load Current Transformers
External load current transformers expand the current range for use with motors greater than 100 A at full load .
Schneider Electric load current transformers |
Primary |
Secondary |
Inside diameter |
Reference |
|
---|---|---|---|---|---|
mm |
In. |
||||
100 |
1 |
35 |
1.38 |
LT6CT1001 |
|
200 |
1 |
35 |
1.38 |
LT6CT2001 |
|
400 |
1 |
35 |
1.38 |
LT6CT4001 |
|
800 |
1 |
35 |
1.38 |
LT6CT8001 |
-
The LTMTCT3/LTMTCTV3 sensor module accepts 1 A and 5 A secondary signals from external current transformers.
-
The LTMTCT25/LTMTCTV25 sensor module accepts 5 A secondary signals from external current transformers.
-
3 A and 25 A CT to be used for external CT.
For more information on external CT wiring, refer to TeSys Tera Motor Management System Installation Guide – DOCA0356EN.