DOCA0257EN-00

Function Parameter

The function parameter of each protection can be set separately to define the action of the protection function on the system.

Function parameter value

Description

Disable

The protection function is disabled.

Alarm

The protection function is used to signal the alarm conditions.

The alarm is not latched and it is automatically reset when the alarm conditions have disappeared.

Alarm + Trip

The protection function is used to signal the alarm conditions and to stop the motor in the trip conditions.

Trip

The protection function is used to stop the motor in the trip conditions. The trip conditions are defined in the description of each protection function.

The trip is latched and must be reset according to the Reset mode set for protection function.

Detection of Alarm

LTMT main unit detects the alarm:

  • After the parameter value crosses the alarm threshold.

  • In 30 ms of time after the parameter value crosses the alarm threshold.

Detection of Pickup and Trip

LTMT main unit detects:

  • Pickup, after the parameter value crosses the pickup threshold.

  • Pickup in 30 ms of time, after the parameter value crosses the pickup threshold.

  • Trip, after the parameter value crosses the pickup threshold and remain above the pickup threshold for configured time delay.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?