Calculated Ground Fault
Description
The ground current is an imbalanced current flowing through the neutral of the three-phase system. In normal conditions, the ground current is negligible or null. It is present only when a ground fault occurs.
![]() |
---|
IMPROPER TRIP DETECTION
Failure to follow these instructions will result in death or serious injury.
|
The ground current is calculated internally by the LTMTCT/LTMTCTV sensor module. The calculated ground fault protection function generates the following signals:
-
Alarm: Calculated ground current goes above the alarm level.
-
Trip: Calculated ground current goes above the pickup level for the specified time delay.
The protection function can be disabled when the motor is in Start state, to avoid nuisance tripping.
-
Calculated ground fault protection is not applicable in single-phase mode.
-
Hysteresis is not applicable for calculated ground current by setting less than 10% of FLC.
Parameter Setting
The calculated ground fault protection function has the following configurable settings:
Parameter |
Setting range |
Default value |
---|---|---|
Function |
|
Trip |
Pickup |
10–500% of IFLC in step of 1% |
20% of IFLC |
Time Delay |
0.05–600.00 s in step of 0.01 s |
0.2 s |
Alarm Level |
10–500% of IFLC in step of 1% |
20% of IFLC |
Reset Mode |
|
DI + Reset Key |
Auto-Reset Delay (applicable only if Reset mode is Auto) |
0–6000.0 s in step of 0.1 s |
0.0 s |
Function While Motor Starting |
|
Disable |