DOCA0257EN-00

Overview

The TeSys Tera system provides the motor starter functions that helps to reduce the wiring and external components like starters or timers. With the TeSys Tera system motor starter functions, the motor can be directly controlled through the contactors.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?