Name Plate
![]() |
---|
UNINTENDED EQUIPMENT OPERATION
The application of this product requires expertise in
the design and programming of control systems. Only personnel with
such expertise should be allowed to program, install, configure, alter
and apply this product. Follow all local and national safety codes
and standards.
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The system settings can be set up using following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.
-
The LTMTCUF control operator unit
-
A PLC or DCS through the communication network.
Parameter name |
Setting range | Default value |
---|---|---|
Tag |
MMR0000001 |
MMR0000001 |
Nominal Power |
0.1–6553.5 KW |
0.1 KW |
Load Type |
|
Motor |
Number of Phases |
|
Three Phase |
Nominal Power
Nominal power value entered in name plate menu is reference for all power related protection.
Load Type
TeSys Tera system supports Motor (inductive) and Heater (resistive) load types. You can configure the load type base on the load.
The default load type is Motor, that enables full functionality of TeSys Tera system based on the device configuration.
The following protection functions are disabled in heater load type:
-
Thermal Overload
-
Locked Rotor
-
Stall Rotor
-
Excessive Start Time
-
Auto Restart
-
Maximum Number of Starts
-
Anti-Backspin Timer
Number of Phases
Select Three-Phase setting for three-phase motor, and Single-Phase setting for single phase motor.