Temperature Measurement
The TeSys Tera system supports maximum 1 temperature inputs for LTMT main unit.
Temperature Measured by LTMT Main Unit
The LTMT main unit temperature input can be connected to a 2-wire temperature sensor.
One of the following types of temperature sensors can be used:
-
PT100
-
Binary PTC
Characteristic |
PT100 temperature sensor |
Binary PTC resistance temperature sensor |
---|---|---|
Range |
0 to 180 °C |
500 to 4000 Ω |
Resolution |
0.1 °C |
1 Ω |
Refresh interval |
500 ms |
500 ms |