DOCA0257EN-00

Voltage Imbalance

Description

The line voltage imbalance function displays the maximum percentage of deviation between the average voltage and the individual line voltages.

The three-phase voltage imbalance is calculated using formula:

Where,

  • VLx= Maximum deviated line voltage from average voltage

  • Vavg = Average voltage of the three phases

NOTE: Not applicable in single-phase mode.

Characteristics

The line voltage imbalance function has the following characteristics:

Characteristic

Value

Unit

%

Accuracy

+/– 1.5%

Resolution

1%

Refresh interval

100 ms

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?