DOCA0257EN-00

Thermal Overload

Description

The thermal overload is a condition where current higher than the rated value flows to the motor resulting in excessive heating of the motor. Rapid motor heating occurs during the overload, acceleration time, and locked rotor condition. The LTMT main unit computes the thermal memory (TM) as per the motor running current.

The thermal overload protection function generates the following signals:

  • Alarm: Thermal memory goes above the alarm level.

  • Trip: Thermal memory reaches to 100%.

  • Thermal Inhibit: When the motor is stopped and thermal memory is above the start thermal inhibit level.

The following graph shows the thermal overload protection curve:

Trip Time Chart

The thermal overload protection function supports different trip classes and service factor setting. The following tables shows the thermal overload protection trip time with respect to motor current, trip class setting, and service factor setting.

Service factor

Motor current (x IFLC)

Trip time (s)

Class 5

Class 10

Class 15

Class 20

Class 25

Class 30

Class 35

Class 40

1.00

7.20

3.46

6.91

10.37

13.83

17.29

20.74

24.20

27.66

6.00

5.00

10.00

15.00

20.00

25.00

30.00

35.00

40.00

5.00

7.25

14.49

21.74

28.98

36.23

43.47

50.72

57.96

4.00

11.45

22.91

34.36

45.82

57.27

68.73

80.18

91.64

3.00

20.91

41.81

62.72

83.62

104.53

125.43

146.34

167.24

2.00

51.06

102.12

153.18

204.24

255.30

306.36

357.42

408.48

1.50

104.33

208.65

312.98

417.30

521.63

625.95

730.28

834.60

1.00

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.05

7.20

3.82

7.63

11.45

15.26

19.08

22.89

26.71

30.52

6.00

5.52

11.04

16.56

22.08

27.60

33.12

38.64

44.16

5.00

8.01

16.01

24.02

32.02

40.03

48.03

56.04

64.04

4.00

12.67

25.34

38.02

50.69

63.36

76.03

88.70

101.37

3.00

23.19

46.39

69.58

92.78

115.97

139.16

162.36

185.55

2.00

57.23

114.46

171.69

228.92

286.15

343.38

400.61

457.84

1.50

119.51

239.02

358.53

478.04

597.55

717.06

836.58

956.09

1.05

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.10

7.20

4.19

8.38

12.58

16.77

20.96

25.15

29.34

33.54

6.00

6.07

12.14

18.20

24.27

30.34

36.41

42.48

48.55

5.00

8.81

17.61

26.42

35.22

44.03

52.83

61.64

70.44

4.00

13.96

27.91

41.87

55.83

69.79

83.74

97.70

111.66

3.00

25.63

51.25

76.88

102.51

128.13

153.76

179.38

205.01

2.00

63.94

127.88

191.82

255.76

319.70

383.64

447.58

511.53

1.50

136.97

273.94

410.91

547.88

684.85

821.82

958.79

1095.76

1.10

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.15

7.20

4.59

9.17

13.76

18.35

22.93

27.52

32.11

36.69

6.00

6.64

13.29

19.93

26.57

33.22

39.86

46.50

53.14

5.00

9.65

19.29

28.94

38.59

48.23

57.88

67.53

77.17

4.00

15.31

30.62

45.94

61.25

76.56

91.87

107.19

122.50

3.00

28.21

56.42

84.62

112.83

141.04

169.25

197.46

225.67

2.00

71.25

142.49

213.74

284.98

356.23

427.47

498.72

569.97

1.50

157.29

314.58

471.87

629.16

786.44

943.73

1101.02

1258.31

1.15

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.20

7.20

5.00

10.00

15.00

20.00

25.00

30.00

35.00

40.00

6.00

7.25

14.49

21.74

28.98

36.23

43.47

50.72

57.96

4.00

16.74

33.48

50.22

66.96

83.70

100.43

117.17

133.91

3.00

30.95

61.89

92.84

123.78

154.73

185.67

216.62

247.57

2.00

79.21

158.42

237.63

316.84

396.05

475.26

554.48

633.69

1.50

181.33

362.66

543.99

725.32

906.66

1087.99

1269.32

1450.65

1.20

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.25

7.20

5.43

10.86

16.30

21.73

27.16

32.59

38.02

43.46

6.00

7.88

15.75

23.63

31.50

39.38

47.25

55.13

63.01

5.00

11.45

22.91

34.36

45.82

57.27

68.73

80.18

91.64

4.00

18.24

36.48

54.72

72.95

91.19

109.43

127.67

145.91

3.00

33.85

67.69

101.54

135.38

169.23

203.07

236.92

270.76

2.00

87.91

175.83

263.74

351.65

439.57

527.48

615.40

703.31

1.50

210.43

420.87

631.30

841.74

1052.17

1262.61

1473.04

1683.47

1.25

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.30

7.20

5.88

11.77

17.65

23.53

29.41

35.30

41.18

47.06

6.00

8.53

17.07

25.60

34.14

42.67

51.20

59.74

68.27

5.00

12.42

24.85

37.27

49.69

62.12

74.54

86.96

99.38

4.00

19.81

39.63

59.44

79.25

99.07

118.88

138.69

158.50

3.00

36.91

73.83

110.74

147.66

184.57

221.49

258.40

295.31

2.00

97.45

194.90

292.35

389.80

487.25

584.70

682.15

779.59

1.50

246.84

493.68

740.52

987.37

1234.21

1481.05

1727.89

1974.73

1.30

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.35

7.20

6.35

12.70

19.06

25.41

31.76

38.11

44.47

50.82

6.00

9.22

18.44

27.66

36.88

46.10

55.32

64.55

73.77

5.00

13.43

26.87

40.30

53.74

67.17

80.61

94.04

107.48

4.00

21.46

42.93

64.39

85.86

107.32

128.78

150.25

171.71

3.00

40.16

80.32

120.48

160.64

200.80

240.97

281.13

321.29

2.00

107.93

215.87

323.80

431.73

539.67

647.60

755.54

863.47

1.50

294.76

589.52

884.28

1179.04

1473.80

1768.56

2063.32

2358.08

1.35

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.40

7.20

6.84

13.68

20.52

27.36

34.20

41.04

47.89

54.73

6.00

9.94

19.87

29.81

39.75

49.68

59.62

69.55

79.49

5.00

14.49

28.98

43.47

57.96

72.45

86.95

101.44

115.93

4.00

23.19

46.39

69.58

92.78

115.97

139.16

162.36

185.55

3.00

43.59

87.19

130.78

174.38

217.97

261.56

305.16

348.75

2.00

119.51

239.02

358.53

478.04

597.55

717.06

836.58

956.09

1.50

363.64

727.28

1090.92

1454.56

1818.19

2181.83

2545.47

2909.11

1.40

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.45

7.20

7.35

14.70

22.05

29.39

36.74

44.09

51.44

58.79

6.00

10.68

21.36

32.04

42.72

53.40

64.08

74.77

85.45

5.00

15.59

31.18

46.78

62.37

77.96

93.55

109.14

124.74

4.00

25.00

50.01

75.01

100.02

125.02

150.03

175.03

200.04

3.00

47.22

94.45

141.67

188.89

236.12

283.34

330.56

377.79

2.00

132.36

264.73

397.09

529.45

661.82

794.18

926.54

1058.91

1.50

483.63

967.26

1450.89

1934.52

2418.15

2901.78

3385.41

3869.04

1.45

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

1.50

7.20

7.88

15.75

23.63

31.50

39.38

47.25

55.13

63.01

6.00

11.45

22.91

34.36

45.82

57.27

68.73

80.18

91.64

5.00

16.74

33.48

50.22

66.96

83.70

100.43

117.17

133.91

4.00

26.90

53.80

80.69

107.59

134.49

161.39

188.29

215.19

3.00

51.06

102.12

153.18

204.24

255.30

306.36

357.42

408.48

2.00

146.73

293.45

440.18

586.90

733.63

880.35

1027.08

1173.81

1.50

No trip

No trip

No trip

No trip

No trip

No trip

No trip

No trip

Parameter Settings

CAUTION
HAZARD OF MOTOR OVERHEATING
The Motor Trip Class parameter must be set to the thermal heating characteristics of the motor. Refer to the motor manufacturers instructions before setting this parameter.
Failure to follow these instructions can result in injury or equipment damage.

The thermal overload protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Alarm

  • Alarm + Trip

  • Trip

  • Disable

Alarm + Trip

Service Factor

1.00–1.50 in step of 0.05

1.15

Trip Class

5, 10, 15, 20, 25, 30, 35, 40

10

Alarm Level

80–100% of thermal memory in step of 5%

80% TM

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

Auto

Thermal Reset Level

30–95% of thermal memory in step of 5%

90% TM

Start Inhibit Level

5–100% of thermal memory in step of 5%

90% TM

Auxiliary Fan

  • Disable

  • Enable

Disable

Cool Down Function

  • Disable

  • Enable

Disable

Cool Down Time

0.0–6000.0 s in step of 0.1 s

0.0 s

Pause Function

  • Disable

  • Enable

Disable

Pause Time

0.0–6000.0 s in step of 0.1 s

0.0 s

Block Function

  • Disable

  • Enable

Disable

Block Level

80–95% of thermal memory in step of 5%

80%

Block Time

0.0–6000.0 s in step of 0.1 s

0.0 s

NOTE: When thermal overload protection is disabled, the thermal memory will increase and thermal inhibit will appear.

Service Factor

Service factor of the motor is configurable from 1.00 to 1.50 as per the motor name plate.

Trip Class

Select the trip class as per the motor characteristics. The LTMT main unit provides thermal overload protection for eight different trip classes – Class 5, Class 10, Class 15, Class 20, Class 25, Class 30, Class 35, Class 40.

Refer to Trip Time Chart for selection of trip class and service factor.

Alarm Level

Alarm level of thermal overload protection is configurable from 80% to 100% of thermal memory. The LTMT main unit generates the alarm signal once the thermal memory goes beyond the alarm level.

Thermal Reset Level

Thermal overload trip can be reset if the thermal memory goes below the thermal reset level.

Start Inhibit Level

Start inhibit level is used to detect the thermal inhibit condition. If the thermal memory goes above the start inhibit level, the thermal inhibit cause is set.

NOTE: When the motor stops, thermal inhibit will appear.

Cool Down Function

Cool down function allows you to reset the thermal memory with configured cool down time.

If the cool down function is enabled and motor is tripped due to thermal overload, thermal memory resets to zero after cool down time has elapsed.

Pause Function

Pause function allows you to reset the thermal memory with the configured pause time, if the motor is not tripped due to thermal overload.

If the pause function is enabled and the motor is not tripped due to thermal overload, thermal memory will reset to zero after the pause time has elapsed.

Block Function

Block function allows you to block the thermal overload protection for the configured block time during the motor start. This function blocks the thermal memory (TM) at the block level. For more information, refer to the below graphical representation.

A Motor stop
B Block time
C Block level

Auxiliary Fan

If the auxiliary fan is enabled, thermal memory will cool down four times faster. This mode is not suitable with cool down function and pause function.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?