DOCA0257EN-00

Thermal Time to Trip

Description

The LTMT main unit displays the time to trip for thermal protection. Based on thermal memory, the LTMT main unit calculates the time remaining before tripping of the thermal protection.

Characteristics

Characteristic

Value

Unit

s

Resolution

1 s

Refresh interval

1 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?