RMS Voltage
Description
The line-to-line voltages function provides the RMS value of the phase-to-phase voltage (VL1–L2, VL2–L3, and VL3–L1):
-
VL1–L2 voltage: Phase 1 to Phase 2 RMS voltage
-
VL2–L3 voltage: Phase 2 to Phase 3 RMS voltage
-
VL3–L1 voltage: Phase 3 to Phase 1 RMS voltage
In single-phase mode:
VL1 voltage: Phase to neutral RMS voltage
Characteristics
Characteristic |
Value |
---|---|
Unit |
Volts (V) |
Resolution |
0.1 V |
Refresh interval |
20 ms |