Communication Ports
The LTMT main unit has the following kinds of communication ports:
-
Modbus RTU Communication Port
-
PROFIBUS DP Communication Port
Modbus RTU Communication Port
The LTMT main unit with Modbus RTU communication is connected to the Modbus field terminals by using a 4-terminal connector.
For more information on wiring and connections, refer to TeSys Tera Motor Management System Modbus RTU Communication Guide – DOCA0355EN
PROFIBUS DP Communication Port
The LTMT main unit with PROFIBUS DP communication can be connected in the PROFIBUS DP daisy chain using two different connectors. In the LTMT main unit, standard DB9 connector is used for conventional method for PROFIBUS DP network. It can be achieved, by looping terminal available for PROFIBUS DP connection.
The maximum data speed with the different connectors are mentioned below.
The PROFIBUS DP 4-terminal connector has the following pin assignments:
Terminal |
Signal |
Description |
---|---|---|
A | RD-/TD- | Negative data transmission (RD-/ RD-) |
B | RD+/TD+ | Positive data transmission (RD+/ RD+) |
– |
Shielded earth |