DOCA0257EN-00

Short Time Overcurrent

Description

The TeSys Tera system provides the definite time short time overcurrent protection function.

The short time overcurrent protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes above the alarm level.

  • Trip: Any of the three-phase currents of the motor goes above the pickup level for the specified time delay.

WARNING
UNINTENDED EQUIPMENT OPERATION
  • Starter function do not stop the motor by de-energizing the contactor output on occurrence of short time overcurrent trip.
  • Configure the separate digital output for short time overcurrent trip, to control circuit breaker.
  • Common trip signal do not trip in case of short time over current.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Parameter Setting

The short time protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Pickup

100–1000% of IFLC in step of 1%

100% of IFLC

Time Delay

0.05–10.00 s in step of 0.01 s

0.05 s

Alarm Level

100–1000% of IFLC in step of 1%

100% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?