DOCA0257EN-00

Average Current

Description

The LTMT main unit calculates the RMS value of the average current using the measured line currents.

Characteristics

Characteristic

Value

Unit

Ampere (A)

Resolution

0.001 A

Refresh interval

20 ms

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?