Digital Inputs
![]() |
---|
UNINTENDED MACHINE OPERATION
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
The TeSys Tera system supports maximum of 24 digital inputs:
-
Four digital inputs on LTMT main units.
-
Up to 20 digital inputs with LTMT expansion units.
Input Configuration
The configuration of the digital inputs can be made through one of the following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.
-
The LTMTCUF control operator unit.
-
A PLC or DCS through the communication network.
Each digital input has the following parameters:
Parameter |
Setting range |
---|---|
Trigger type |
|
Validation time |
0 to 60000 ms in step of 10 ms |
Input source |
See list in input assignment |
The digital inputs are set by default depending on the motor starter type selected.
Input Type
The Active type and Validation time (t) parameters defines how the physical information connected to the input (A) is converted in the digital input information (B) processed by the LTMT main unit.
Input Assignment
Input source |
Description |
---|---|
Other |
Do not use, reserved for future programmable feature. |
Trip Reset DI |
Used to configure the digital input for trip reset. |
Breaker Close DI |
Used in custom logic to customize the application. This input is not directly used by the motor starter logic. |
Breaker Open DI |
Used in custom logic to customize the application. This input is not directly used by the motor starter logic. |
Local-START> DI |
Local Forward Start command. Used by the motor starter logic as per the selected starter type. |
Local-START>> DI |
Local Fast Forward (Forward High speed) Start command. Used by the motor starter logic as per the selected starter type. |
Local-STOP DI |
Local Stop command. Used by the motor starter logic as per the selected starter type. |
Local-START< DI |
Local Reverse Start command. Used by the motor starter logic as per the selected starter type. |
Local-START<< DI |
Local Fast Reverse (Reverse High speed) Start command. Used by starter module as per the selected starter type. |
Remote-START> DI |
Remote Forward Start command. Used by the motor starter logic as per the selected starter type. |
Remote-START>> DI |
Remote Fast Forward (Forward High speed) Start command. Used by the motor starter logic as per the selected starter type. |
Remote-STOP DI |
Remote Stop command. Used by the motor starter logic as per the selected starter type. |
Remote-START< DI |
Remote Reverse Start command. Used by the motor starter logic as per the selected starter type. |
Remote-START<< DI |
Remote Fast Reverse (Reverse High speed) Start command. Used by the motor starter logic as per the selected starter type. |
Interlock 1 |
Up to 12 digital inputs can be configured as interlocks. These interlock inputs are used by:
|
Interlock 2 |
|
Interlock 3 |
|
Interlock 4 |
|
Interlock 5 |
|
Interlock 6 |
|
Interlock 7 |
|
Interlock 8 |
|
Interlock 9 |
|
Interlock 10 |
|
Interlock 11 |
|
Interlock 12 |
|
Contactor open DI |
Used in custom logic to customize the application. This input is not directly used by the motor starter logic. |
Run DI |
Used by the motor starter logic to check the contactor/RUN feedback. |
Block Input |
Used for co-ordination purpose. If the block input is present, the TeSys Tera system will block the trip output. |
Logic test DI |
Used to perform logic tests. |
Mode selection 1 |
Used to select the operating mode: Local 1, Local 2 , Local 3 or Remote. |
Mode selection 2 |
|
Forced start |
Used by forced start function. |
Forced stop |
Used by the motor starter logic as forced stop. |
Self test without trip |
Used by test function. |
Self test with trip |
Used by test function. |
None |
_ |