DOCA0257EN-00

Device Configuration

WARNING
UNINTENDED EQUIPMENT OPERATION
  • The application of this product requires expertise in the design and programming of control systems. Only personnel with such expertise should be allowed to program, install, configure, alter and apply this product. Follow all local and national safety codes and standards.
  • Change in Device Configuration can cause short circuit or turn on power supply to the load.
  • Check if appropriate wiring is done according to the Device Configuration.
  • Ensure that the three-phase or single phase power supply is cut off to the motor, and control supply to the inputs and outputs is cut off to the expansion units while changing the Device Configuration.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The configuration of the TeSys Tera system can be set up using following interfaces:

  • A PC running the TeSys Tera DTM embedded in a FDT container such as SoMove software.

  • The LTMTCUF control operator unit.

  • A PLC or DCS through the communication network.

Parameter Setting

Parameter name

Setting range

Default value

LTMTCT/LTMTCTV sensor module type

  • LTMTCT3T

  • LTMTCTV3T

  • LTMTCT25T

  • LTMTCTV25T

  • LTMTCT100T

  • LTMTCTV100T

  • LTMTCTV3UT

  • LTMTCTV25UT

  • LTMTCTV100UT

LTMTCTV25T

LTMT expansion unit 1 type

  • None

  • LTMTIN42FM

  • LTMTIN42BD

None

LTMT expansion unit 2 type

  • None

  • LTMTIN42FM

  • LTMTIN42BD

None

LTMT expansion unit 3 type

  • None

  • LTMTIN42FM

  • LTMTIN42BD

None

LTMT expansion unit 4 type

  • None

  • LTMTIN42FM

  • LTMTIN42BD

None

LTMT expansion unit 5 type

  • None

  • LTMTIN42FM

  • LTMTIN42BD

None

LTMT main unit temperature sensor type

  • None

  • PT100

  • PTC

None

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?