Live Swap: Add, Remove, or Replace a Power Module
DISCLAIMER:
-
Electrical equipment should be installed, operated, serviced, maintained, replaced, or have similar work carried out on it only by suitably qualified, trained, experienced, and competent personnel who hold any necessary authorizations (e.g. licenses, permits or certifications) to perform such work. All work must be carried out in a way that does not give rise to danger and using appropriate personal protective equipment (PPE).
-
User must ensure compliance with the manufacturer’s instructions and user manual and with all applicable laws, regulations, standards, and guidance when using this equipment and carrying out work or permitting work to be carried out on or near electrical equipment.
-
Neither Schneider Electric nor any of its affiliates shall be liable for any claims, costs, losses, damages, death, or injuries arising out of the improper use of this equipment or any failure to comply with any of the above requirements.
PELIGRO |
|---|
|
Hazard of electric shock, explosion, or arc flash
Si no se siguen estas instrucciones, se producirán lesiones graves o la muerte.
|
ADVERTENCIA |
|---|
|
risk of equipment damage
Si no se siguen estas instrucciones, pueden producirse lesiones graves, muerte o daños
en el equipo.
|
ADVERTENCIA |
|---|
|
Heavy load
Power modules are heavy (54 kg). Use appropriate lifting equipment and trained personnel
to lift and handle the power module. It is recommended to use a scissor
lifting cart or similar appropriate lifting equipment as shown in
this procedure. See the specifications for the recommended scissor
lifting cart below. If no lifting equipment is available, three persons
are required to lift and handle the power module.
Si no se siguen estas instrucciones, pueden producirse lesiones graves, muerte o daños
en el equipo.
|
ADVERTENCIA |
|---|
|
Hazard of injury
Never stack the power modules on top of each other.
Si no se siguen estas instrucciones, pueden producirse lesiones graves, muerte o daños
en el equipo.
|
ATENCIÓN |
|---|
|
Heavy load and potentially hot surface
Use protective gloves and safety shoes when handling the
power modules.
Si no se siguen estas instrucciones, pueden producirse lesiones o daños en el equipo.
|
| AVISO |
|---|
|
Risk of Installation overload
Check and verify that the installation is correctly sized
for the increase in power rating before installing more power modules
in the UPS. Incorrect sizing of the installation can result in an
installation overload. See the installation manual for requirements
for upstream and downstream protection, cable sizes, etc.
Si no se siguen estas instrucciones, pueden producirse daños en el equipo.
|
| AVISO |
|---|
|
Risk of load drop
Check and verify that the remaining power modules can
support the load before removing a power module from the UPS.
Si no se siguen estas instrucciones, pueden producirse daños en el equipo.
|
- Remove an installed power module:
- Set the enable switch to the OFF (unlocked) position. Remove the four screws from the power module and save the screws.
- Use the provided power module tool* to pull the power module out from the power module slot. Place the power module tool as shown.
- Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
- Release the lock by pressing the release button in the right side of the power module and pull the power module out onto an appropriate scissor lifting cart.
- If no replacement power module will be installed: Install a filler plate in front of the empty power module slot. Reuse the screws from the old power module.
- Install a new power module:
- If present, remove the filler plate from the empty power module slot. Save the filler plate for future use and save the screws.
- Use an appropriate lifting cart to lift the power module to the correct height and push the power module into the power module slot.
- Install the four screws in the left and right sides of the power module. Reuse the screws from the filler plate/old power module.
- Set the enable switch on the power module to the ON (locked) position.
The power module will perform a self-test, automatically upgrade the firmware according to the system, and then go online. The UPS operation mode shown on the display will briefly change to Battery operation during the self-test and then return to the previous operation mode.
PELIGRO
ADVERTENCIA
ATENCIÓN