BQT6904400-03

Feeder with Contactor Cubicle (FC)

Figure 1
Feeder with Contactor (FC)


Table 4 Feeder with Contactor Cubicle Dimensions and Weights

Rated voltage (kV)

Dimensions

Rated current of cubicle (A)

315

7.2/12

Width W (mm)

400

Cubicle height H (mm)(1)

2240

Depth D (mm)

1440

Approximate weight (kg)(2)

800

Approximate maximum weight (kg) of CT(3)

25

(1) This dimension excludes cable flanges as well as any compartments placed under the cubicle.

(2) Maximum fully fitted weight of the cubicle including CVX contactor.

(3) 3 CTs per set.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?