Control Unit NIII_Z_1: Check Microswitches OF/SDE/PF/CH
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check that the microswitches delivering the OF/SDE/PF/CH information to the MicroLogic X control unit operate correctly. |
|
Goal |
Verify that the MicroLogic X control unit gets the device status information. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
Checking the Microswitches OF/SDE/PF/CH
Check that the microswitches OF/SDE/PF/CH and the control unit are functioning correctly:
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
If the device is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
|
2 |
||
|
3 |
Launch EcoStruxure Power Commission software. |
|
|
4 |
Click Result: A window displays to indicate that the device discovery is in progress. It disappears automatically when the device is discovered. |
|
|
5 |
Click to close the window. |
|
|
6 |
Click to close the window and display the SWITCHBOARD VIEW. |
|
|
7 |
Click the button. |
|
|
8 |
In the section, click the Device tab. |
|
|
9 |
If no MCH gear motor is installed in the device, charge the device by using the spring charging handle. |
|
|
10 |
Check that data is as follows:
|
If a status of the device is not correct:
|
|
11 |
Manually close the device. |
|
|
12 |
Check that data is as follows:
|
If a status of the device is not correct, see corrective action in step 9. |
|
13 |
In the tab, click the button to trip the device. |
|
|
14 |
Read carefully the safety message that displays then click . |
|
|
15 |
You are prompted to provide the password:
|
|
|
16 |
In the window, click . |
|
|
17 |
Check that data is as follows:
|
If a status of the device is not correct, see corrective action in step 9. |
|
18 |
Reset the device by pressing the blue button. |
|
|
19 |
If no MCH gear motor is installed in the device, charge the device by using the spring charging handle. |
|
|
20 |
Check that data is as follows:
|
If a status of the device is not correct, see corrective action in step 9. |
|
21 |
Exit EcoStruxure Power Commission software. |
DANGER