Breaking Unit NIII_Z_2: Check Mounting of Arc Chutes and Filter Cleanliness
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify the breaking performance of the device during a short-circuit. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
This procedure is not applicable to the MasterPacT MTZ1 H3 devices because arc chutes are not removable on MasterPacT MTZ1 H3 devices. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected and Removed from chassis |
Checking Mounting of Arc Chutes and Filter Cleanliness
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check the presence of all screws on the arc chutes (except for MasterPacT MTZ1 H3). NOTE: The
presence of all screws is mandatory to help to prevent the ionized
gas from leaking through the edges of the arc chute.
|
If screws are damaged or missing, contact your Schneider Electric Services representative. |
|
2 |
Unscrew the screws on the arc chutes (except for MasterPacT MTZ1 H3), then tighten them to the recommended value using a torque wrench:
|
If a screw cannot be tightened at the recommended value, contact your Schneider Electric Services representative. |
|
3 |
Use a vacuum cleaner to remove the dust deposited on the filters. NOTE: To avoid soiling
the filters:
|
If the filters are still dirty (for example, greasy compound), replace the arc chutes (refer to MasterPacT MTZ - Arc Chute - Instruction Sheet). Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
DANGER
DANGER