Auxiliaries NIII_Z_1: Check Operation of Indication Contacts (OF, PF)
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the operation of indication contacts OF and PF. |
|
Goal |
Verify electrical continuity of the installed contacts and contact robustness. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
OF Indication Contact Wiring Diagram
The number of OF indication contacts depends on the device type:
Checking Operation of OF Indication Contacts
Do this procedure for each OF indication contact of the device.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the device is in the open position. |
|
|
2 |
Check electrical continuity between terminals:
If additional OF blocks are installed, check all terminals. |
In case of electrical non-continuity between terminals:
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
3 |
Close the device. |
|
|
4 |
Check electrical continuity between terminals:
If additional OF blocks are installed, check all terminals. |
In case of electrical non-continuity between terminals, see the corrective action concerning electrical continuity above. |
PF Ready-To-Close Contact Wiring Diagram
Checking Operation of PF Ready-To-Close Contact
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Close the device. |
|
|
2 |
Verify that the PF contact indicates that the device is not ready-to-close:
|
In case of electrical non-continuity between terminals 251-254, or electrical continuity between terminals 251-252:
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
3 |
Open the device. |
|
|
4 |
Charge the mechanism. |
|
|
5 |
The device is ready-to-close. |
|
|
6 |
Verify that the PF contact indicates that the device is ready-to-close:
|
In case of electrical non-continuity between terminals 251-252, or electrical continuity between terminals 251-254, see the corrective action concerning electrical continuity above. |
DANGER