Chassis NII_Z_2: Check IBPO Racking Interlock (MasterPacT MTZ2/MTZ3)
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check IBPO racking interlock between racking handle and opening pushbutton. Check disconnection and connection of a drawout MasterPacT MTZ2/MTZ3 device when the IBPO racking interlock is installed. |
|
Goal |
Verify that the IBPO racking interlock operates correctly and does not allow connection and disconnection of the device without additional action. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
Racking handle |
|
MasterPacT MTZ2/MTZ3 - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - User Guide |
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Charged |
Connected |
Checking Device Disconnection with IBPO Racking Interlock Accessory (MasterPacT MTZ2/MTZ3)
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the equipment door is closed. |
|
|
2 |
Check that the racking handle cannot be inserted into the racking handle socket. |
|
|
3 |
Press and hold the opening pushbutton to allow insertion of the racking handle into the racking handle socket. |
If the racking handle cannot be inserted into the racking handle socket:
If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
Rack-out the device from connected to test position. When the test position is reached, the mechanism blocks the racking handle and the position release button pops out. NOTE: If needed, refer to device racking operations as
per procedure Chassis NII_Z_1.
|
|
|
5 |
Remove the racking handle from the racking handle socket. |
Checking Device Connection with IBPO Racking Interlock Accessory (MasterPacT MTZ2/MTZ3)
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the racking handle cannot be inserted into the racking handle socket. |
|
|
2 |
Press and hold the opening pushbutton to allow insertion of the racking handle into the racking handle socket. |
|
|
3 |
Rack-in the device from test to connected position. When the connected position is reached, the mechanism blocks the racking handle and the position release button pops out. NOTE: If needed, refer to device racking
operations as per procedure Chassis NII_Z_1.
|
|
|
4 |
Remove the racking handle from the racking handle socket, and then put it back into its storage space. |
|
|
5 |
Reinstall the VPOC racking interlock if removed previously. |
DANGER