Breaking Unit NIII_Z_1: Check the Condition of the Breaking Unit
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the condition of the elements of the breaking unit:
|
|
Goal |
Verify that all subassemblies participating in arc extinction for rated and short-circuit currents correctly operate. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
This procedure is not applicable to the MasterPacT MTZ1 H3 devices because arc chutes are not removable on MasterPacT MTZ1 H3 devices. |
|
Necessary tools |
Torque wrench |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Removed from chassis |
Checking Separator Plates
Execute the following procedure for each arc chute and one arc chute at a time.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
NOTE: Do not remove the other arc chutes.
|
|
|
2 |
NOTE: Do not turn the arc chute upside down when
removing it so that the fixing screws do not fall in the arc chamber.
|
|
|
3 |
Check the separator plates: the separator plates must not be corroded, they may be blackened but must not be significantly damaged. |
If damage is extensive, replace the arc chute (refer to MasterPacT MTZ - Arc Chute - Instruction Sheet). |
|
4 |
Compare the number of electrical operating cycles with the maximum values indicated in MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide . |
Depending on the number of electrical operating cycles and state of separator plates, replace the arc chute (refer to MasterPacT MTZ - Arc Chute - Instruction Sheet). Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
Checking Surface of Arcing Contact and Fixed and Moving Contact Tips
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
With the arc chute removed, check the surface of the arcing contact and fixed contact tips. |
|
|
2 |
Check the surface of the moving contact tips. |
|
|
3 |
Compare the number of operating cycles at In with the maximum values indicated in MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide . |
If the limit has been reached, contact your Schneider Electric Services representative to replace the breaking unit. Example: For MasterPacT MTZ2 16 H1, the breaking unit must be changed when 1,000 cycles are reached. |
Checking Contact-Wear Indicator On MasterPacT MTZ1
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Close the device |
|
|
2 |
|
If d < 1 mm, the contact tips are worn. Contact your Schneider Electric Services representative to replace the breaking unit. |
Checking Contact-Wear Indicator On MasterPacT MTZ2/MTZ3
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Close the device. |
|
|
2 |
Check that the channel is covered by the arcing horn for Type A devices:
|
If the channel is no longer covered, the contact tips are worn. Contact your Schneider Electric Services representative to replace the breaking unit. |
|
3 |
Checking Sides of Arc Chamber
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
If the sides are burned or punctured, contact your Schneider Electric Services representative to replace the breaking unit. |
|
|
2 |
Put the arc chute back in place. NOTE: For MasterPacT MTZ1: Make sure that the arrow on the top
of the arc chute points towards the mechanism.
|
|
|
3 |
Tighten the arc chute fixing screws to the recommended value using a torque wrench:
|
If a screw cannot be tightened at the recommended value, contact your Schneider Electric Services representative. |
|
4 |
Do the procedure from the beginning for another arc chute on the device. |
DANGER
DANGER