Mechanism NIII_Z_1: Check the MCH Gear Motor Charging Time at 0.85 Un
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify the correct operation of the MCH gear motor. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
Connect the MCH gear motor to a power supply. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
MCH Gear Motor Charging Time Definition
The charging time is the time elapsed between the closing order and the moment when the mechanism is fully charged.
The charging time during closing operation and opening/closing operation does not exceed 6 seconds.
Checking the MCH Gear Motor Charging Time During Device Closing
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
When using the adjustable external power supply, take
all suitable measures to protect against electric shock.
Failure to follow these instructions will result in death or serious injury.
|
Before starting this check, it is advisable to verify that the device charges electrically with MCH gear motor as per procedure Mechanism NII_Z_2.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Disconnect supply wires B1 and B2 (and B3 if connected) so that the MCH gear motor is not connected to a power supply. |
|
|
2 |
Connect terminals B1 and B2 to the adjustable external power supply. |
|
|
3 |
Set the voltage to 0.85 Un (minimum Un if the setting is for a range of voltages). The MCH gear motor charges the mechanism. The indicators show that the device is open and the mechanism is charged and ready-to-close. |
|
|
4 |
Press the closing pushbutton and start the stopwatch. The device closes and the mechanism is automatically charged. |
|
|
5 |
Stop the stopwatch when the mechanism is charged and not ready-to-close. The charging time should be less than 6 seconds. |
If the charging time exceeds 6 seconds:
If the problem persists, contact your Schneider Electric Services representative to replace the breaking unit. |
Checking the MCH Gear Motor Charging Time During Device Closing/Opening Sequence
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Open the device. |
|
|
2 |
Press the closing pushbutton and immediately the opening pushbutton, and then start the stopwatch. |
|
|
3 |
Stop the stopwatch when the indicators show that the device is open and the mechanism is charged and ready-to-close. The charging time should be less than 6 seconds. |
If the charging time exceeds 6 seconds:
If the problem persists, contact your Schneider Electric Services representative to replace the breaking unit. |
Reconnecting the MCH Gear Motor
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Reconnect the supply wires (B1, B2, and B3 if present) as they were before executing the procedure. |
|
|
2 |
Open and close the device to check that the MCH gear motor operates properly. |
DANGER