Chassis NIII_Z_2: Check Operation of Safety Shutters
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify that the safety shutters operate correctly and prevent access to the power circuit when the device is removed from the chassis. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Removed from chassis |
Checking Safety Shutter Operation for MasterPacT MTZ1, MTZ2, and for MTZ3 Before 09/2022
Execute the following procedure for each safety shutter.
Checking Safety Shutter Operation for MasterPacT MTZ3 After 09/2022
From 09/2022, each MTZ3 safety shutter protects the top and bottom chassis clusters of one phase. Prior to this date, one safety shutter protected the top chassis clusters of all phases, and one safety shutter protected the bottom chassis clusters of all phases.
Execute the following procedure for the safety shutter mechanism of each phase.
Checking Shutter Padlocking with the VIVC Locking Accessory for MasterPacT MTZ2, and for MTZ3 Before 09/2022
Before starting this check, verify that the VIVC front face shutter position indication and locking accessory is mounted.
The top or bottom safety shutters can be locked individually or together on MasterPacT MTZ2 devices and on MasterPacT MTZ3 devices manufactured before 09/2022.
Safety shutter locking is only possible with the chassis in test or disconnected position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Pull out the right-hand tab. |
If the tab cannot be pulled out, check that the locking accessory is correctly installed (refer to MasterPacT MTZ2/MTZ3 - VIVC Front Face Shutter Position Indication and Locking - Instruction Sheet). If the locking accessory is damaged, replace it. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
2 |
Insert the padlock in this tab. |
|
|
3 |
Check that it is not possible to press the shutter actuator of the bottom safety shutter. The bottom safety shutter must remain closed. |
If the shutter actuator can be pressed and/or the safety shutter can be opened, remove and replace the shutter. If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
Check that the racking handle cannot be inserted. |
If the racking handle can be inserted, contact your Schneider Electric Services representative |
|
5 |
Remove the padlock. |
|
|
6 |
Pull out the left-hand tab. |
|
|
7 |
Insert the padlock in this tab. |
|
|
8 |
Check that it is not possible to press the shutter actuator of the top safety shutter. The top safety shutter must remain closed. |
If the shutter actuator can be pressed and/or the safety shutter can be opened, remove and replace the shutter. If the problem persists, contact your Schneider Electric Services representative. |
|
9 |
Check that the racking handle cannot be inserted. |
If the racking handle can be inserted, contact your Schneider Electric Services representative |
|
10 |
Remove the padlock. |
Checking Shutter Padlocking with the VIVC Locking Accessory for MasterPacT MTZ3 After 09/2022
Before starting this check, verify that the VIVC front face shutter position indication and locking accessory is mounted.
The VIVC locking accessory locks all safety shutters together on MasterPacT MTZ3 devices manufactured after 09/2022.
Safety shutter locking is only possible with the chassis in test or disconnected position.
DANGER
DANGER