Mechanism NII_Z_2: Charge the Device Electrically with MCH Gear Motor
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify that the device charges electrically. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
Connect the MCH gear motor to the power supply. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
MCH Gear Motor Wiring Diagram
MCH Gear Motor Charging Time Definition
The charging time is the time elapsed between the closing order and the moment when the mechanism is fully charged.
The charging time during the closing operation does not exceed 6 seconds.
Checking Operation of MCH Gear Motor and CH Contact
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Remove the MCH gear motor power supply. |
|
|
2 |
Do an opening/closing/opening cycle to discharge the mechanism. |
|
|
3 |
With the device in the open position and the mechanism discharged, check electrical continuity between terminals B1-B2, and electrical non-continuity between terminals B1-B3. |
In case of electrical non-continuity between terminals B1-B2, or electrical continuity between terminals B1-B3:
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
Manually charge the mechanism. |
|
|
5 |
Reconnect the MCH gear motor power supply. |
|
|
6 |
Start the stopwatch while pressing the closing pushbutton. The device closes and the mechanism is automatically charged. |
If the device does not close, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
7 |
Stop the stopwatch when the mechanism is totally charged. |
|
|
8 |
Check the mechanism charging time: it must not exceed 6 seconds. |
If the charging time exceeds 6 seconds, do the procedure three more times from the beginning. If the charging time does not improve, follow the procedure Mechanism NIII_Z_1 to check the voltage supply of the MCH gear motor. If there is still no improvement, replace the MCH gear motor and measure the charging time again. If the problem persists, contact your Schneider Electric Services representative. |
|
9 |
Check electrical continuity between terminals B1-B3. |
In case of electrical non-continuity between terminals B1-B3, see the corrective action concerning electrical continuity above. |
Checking Number of Charging Operations of MCH Gear Motor From EcoStruxure Power Device App on a Smartphone
You can read the charging motor counter remotely from EcoStruxure Power Device app with Bluetooth Low Energy connection.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Read the value on the mobile application. For information about EcoStruxure Power Device app, refer to MasterPacT MTZ - MicroLogic X Control Unit - User Guide. |
|
|
2 |
Compare the value with the maximum number of charging operations indicated in MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide . |
|
DANGER