Mechanism NIII_Z_3: Check the Number of Device Operating Cycles
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the number of device operating cycles on the CDM operation counter, if present. |
|
Goal |
Verify that the maximum recommended number of operating cycles has not been exceeded. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
– |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
Checking Operating Cycle with the Optional CDM Operation Counter
The CDM operation counter increments each time the device performs an open/close cycle.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Read the value on the CDM operation counter. |
|
|
2 |
Compare the value with the maximum number of mechanical operations indicated in MasterPacT MTZ - IEC Switch-Disconnectors and Circuit Breakers with MicroLogic X Control Unit - Maintenance Guide . |
|
DANGER