Mechanism NII_Z_1: Operate the Device Manually and Electrically
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the operation of:
|
|
Goal |
Verify that the device can be opened/closed manually and electrically. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
Connect the XF/MX/MN voltage releases to the power supply. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
Checking Manual Opening/Closing of the Device
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
For fixed devices equipped with the MCH gear motor, disconnect the auxiliary circuit for the MCH gear motor (terminals B1 and B2). |
|
|
2 |
Manually charge the mechanism by pulling the spring charging handle down six times. |
|
|
3 |
Press the closing pushbutton to close the device. The device closes. |
If the device does not close, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
Check that the indicators show that the device is closed, and the mechanism is discharged. |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
5 |
Check that the CDM operation counter increments. |
If the CDM operation counter does not increment, check it is correctly installed (refer to MasterPacT MTZ - CDM Operation Counter - Instruction Sheet). If the CDM operation counter does not increment and is correctly installed, replace it. |
|
6 |
Charge the mechanism again. Check that the indicators show that the device is closed, and the mechanism is charged and not ready-to-close. |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
7 |
Press the opening pushbutton to open the device. The device opens. |
If the device does not open, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
8 |
Check that the indicators show that the device is open, and the mechanism is charged and ready-to-close. |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
Checking Electrical Closing with the XF Closing Voltage Release
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
When using the adjustable external power supply, take
all suitable measures to protect against electric shock.
Failure to follow these instructions will result in death or serious injury.
|
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Reconnect the auxiliary circuit for the MCH gear motor (terminals B1 and B2). |
|
|
2 |
Press the external pushbutton to close the device. The device closes. |
If the device does not close, it can be due to external conditions. Refer to troubleshooting in the appendix. If the external conditions are correct:
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
3 |
Check that the indicators show that the device is closed and check the mechanism status: |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
Check that the CDM operation counter increments. |
If the CDM operation counter does not increment, check it is correctly installed (refer to MasterPacT MTZ - CDM Operation Counter - Instruction Sheet). If the CDM operation counter is correctly installed, replace it. |
Checking Electrical Opening with the MX Opening Voltage Release
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
When using the adjustable external power supply, take
all suitable measures to protect against electric shock.
Failure to follow these instructions will result in death or serious injury.
|
Execute the following procedure for MX1 then MX2, if connected.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
For drawout devices, check that the device is in the test position. |
|
|
2 |
Press the external pushbutton to open the device. The device opens. |
If the device does not open, it can be due to external conditions. Refer to troubleshooting in the appendix. If the external conditions are correct:
Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
3 |
Check that the indicators show that the device is open and check the mechanism status: |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
Checking Electrical Opening with the MN Undervoltage Release
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
For drawout devices, check that the device is in the test position. |
|
|
2 |
|
|
|
3 |
Press the external pushbutton to close the device. The device closes. |
If the device does not close, check the MN undervoltage release wiring and power supply, and refer to troubleshooting in the appendix. |
|
4 |
|
If the device does not open, replace the MN undervoltage release (refer to MasterPacT MTZ - MN-MX-XF Voltage Releases - Instruction Sheet). Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. If the problem persists, contact your Schneider Electric Services representative. |
|
5 |
Check that the indicators show that the device is open and check the mechanism status: |
If the indicators show different information, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
Checking Opening/Closing of the Device in a Communication Network
If XF/MX communicating voltage releases are installed in the device, do the following procedure to test the close and open controls of the device by using EcoStruxure Power Commission software.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
||
|
2 |
Launch EcoStruxure Power Commission software. |
|
|
3 |
Click Result: A window displays to indicate that the device discovery is in progress. It disappears automatically when the device is discovered. |
|
|
4 |
Click to close the window. |
|
|
5 |
Click to close the window and display the SWITCHBOARD VIEW. |
|
|
6 |
Click the button. |
|
|
7 |
In the section, click the Device tab. |
|
|
8 |
Click to close the device. |
|
|
9 |
Read carefully the safety message that displays then click . |
|
|
10 |
You are prompted to provide the password:
|
|
|
11 |
A message displays when the close operation of the device has completed successfully. Click . |
If the device does not close, refer to troubleshooting in the appendix. |
|
12 |
In data, check that is . |
If the device status is not correct, contact your Schneider Electric Services representative. |
|
13 |
In the window, click to open the device. |
|
|
14 |
Read carefully the safety message that displays then click . |
|
|
15 |
You are prompted to provide the password:
|
|
|
16 |
A message displays when the open operation of the device has completed successfully. Click . |
If the device does not open, refer to troubleshooting in the appendix. |
|
17 |
In data, check that is . |
If the device status is not correct, contact your Schneider Electric Services representative. |
|
18 |
Click the button to disconnect the device from EcoStruxure Power Commission software. |
|
|
19 |
Exit EcoStruxure Power Commission software. |
DANGER