Chassis NIII_Z_3: Clean Chassis and Check Presence of Grease on Chassis
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify the smooth mechanical racking-in and racking-out of the device. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Removed from chassis |
Checking Cleanliness of Internal Parts of Chassis
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Check cleanliness of the internal parts of the chassis. In presence of dust, use a vacuum cleaner to remove it.
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Do not use pressurized cleaning products or products containing
solvents (trichloroethane or trichloroethylene) such as WD40.
Failure to follow these instructions can result in equipment damage.
|
Checking Greasing of Internal Parts of Chassis
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check the color and texture of grease. See parts indicated in the corresponding illustrations for MasterPacT MTZ1 or MasterPacT MTZ2/MTZ3. NOTE:
|
If there is a change in grease (for example, grease is dirty or hardened on the mechanical parts of the chassis), contact your Schneider Electric Services representative. |
|
2 |
Check if the grease on the mechanical parts is applied uniformly on the whole zone concerned. See parts indicated in the corresponding illustrations for MasterPacT MTZ1 or MasterPacT MTZ2/MTZ3. NOTE:
|
|
DANGER
DANGER