Device Locking NII_Z_1: Operate Device Keylocks
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the locking and unlocking of the device with keylocks. |
|
Goal |
Verify the operation of keylocks with the optional VSPO OFF-position locking accessory. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
– |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Closed |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected |
Checking Locking the Device in the Open Position
For devices with two keylocks, execute the following procedure for each keylock. Locking with one key is sufficient to lock the device in the open position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
With the key captive in the keylock, check that the device is not locked. |
If the key is missing or broken, replace the keylock. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
2 |
||
|
3 |
|
If the key does not turn, replace the keylock. |
|
4 |
Remove the key and release the opening pushbutton. NOTE: For MasterPacT MTZ1, the pushbutton remains pushed-in.
|
|
|
5 |
Charge the mechanism to be able to give a closing order. |
|
|
6 |
If the device is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
|
7 |
The device must not close. |
If the problem persists, contact your Schneider Electric Services representative. |
|
8 |
If there is a second key, unlock the device and do the procedure with the second key. |
Checking Device Unlocking
Before starting this check, verify that the device is locked in the open position.
For devices with two keylocks, execute the following procedure for each keylock. Both keys must be inserted in the keylocks to unlock the device.
DANGER