Auxiliaries NIII_Z_5: Check Time Delay of MNR Delayed Undervoltage Release
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the time delay on the MN delay unit at 0.35 Un and 0.7 Un. |
|
Goal |
Verify that the MNR delayed undervoltage release is not activated before the end of the selected time delay. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
Connect the MNR delayed undervoltage release to an external power supply. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Closed |
Discharged |
N/A |
|
Drawout |
Closed |
Discharged |
Test |
Time Delay Definition
The time delay is the time elapsed between the opening order and the moment when the MNR delayed undervoltage release operates.
The time delay does not exceed the delay setting ±15%.
MNR Delayed Undervoltage Release Wiring Diagram
Checking the Time Delay of the MN Delay Unit During Device Opening
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
When using the adjustable external power supply, take
all suitable measures to protect against electric shock.
Failure to follow these instructions will result in death or serious injury.
|
Before starting this check, it is advised to execute a few electrical opening and closing cycles as per procedure Mechanism NII_Z_1.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Disconnect supply wires on the customer terminal block. |
|
|
2 |
Connect the adjustable external power supply according to the corresponding wiring diagram above. NOTE: If possible, the opening time should be measured
using the main connections. If that is not possible, carry out the
measurement on an OF contact.
|
|
|
3 |
Set the external power supply voltage to 0.35 Un. |
|
|
4 |
To start the stopwatch, remove the power supply or issue a delayed opening order. |
|
|
5 |
The device opens when the time delay equals the delay setting on the MN delay unit. The stopwatch stops when the device opens. |
|
|
6 |
Check the time delay on the stopwatch: it must equal the delay setting ±15%. |
If the time delay differs by more than ±15% from the delay unit setting, replace the MN delay unit (refer to MasterPacT MTZ - MN-MX-XF Voltage Releases - Instruction Sheet) and do the procedure again. If the problem persists, contact your Schneider Electric Services representative. |
|
7 |
Reconnect the external power supply to the MNR delayed undervoltage release, and then close the device. |
|
|
8 |
Set the external power supply voltage to 0.7 Un. |
|
|
9 |
To start the stopwatch, remove the power supply or issue a delayed opening order. |
|
|
10 |
The device opens when the time delay equals the delay setting on the MN delay unit. The stopwatch stops when the device opens. |
|
|
11 |
Check the time delay on the stopwatch: it must equal the delay setting ±15%. |
If the time delay differs by more than ±15% from the delay unit setting, replace the MN delay unit (refer to MasterPacT MTZ - MN-MX-XF Voltage Releases - Instruction Sheet) and do the procedure again. If the problem persists, contact your Schneider Electric Services representative. |
|
12 |
Reconnect the customer terminal block according to the initial wiring. |
|
|
13 |
Check that the device electrically closes and opens according to procedure Mechanism NII_Z_1. |
DANGER