Chassis NIII_Z_1: Check Operation of CD, CT, CE Position Contacts and EF Auxiliary Contacts
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Operate the chassis position contacts:
|
|
Goal |
Verify consistency between actual position of the device in the chassis and the indications given by the position contacts. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
|
|
Necessary tools |
Ohmmeter or tester |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected NOTE: It is advisable to check the positions
with the device in the chassis to obtain the correct position of the
actuators.
|
Location of Contacts in the MasterPacT MTZ1 Devices
Location of Contacts in the MasterPacT MTZ2/MTZ3 Devices
Wiring Diagrams of CD, CT, and CE Position Contacts
The following wiring diagrams show the case of a MasterPacT MTZ2/MTZ3 chassis with three CD, three CT, and three CE contacts, that is, the standard configuration without EIFE embedded Ethernet interface. The checking operations are based on this configuration. The availability of the position contacts depends on the customer configuration.
Checking Position Contacts With Device in Disconnected Position
The CD position contacts indicate that the device is in the disconnected position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the device is in the disconnected position. NOTE: If
needed, refer to device racking operations as per procedure
Chassis NII_Z_1.
|
|
|
2 |
Check that the signal is consistent with the device position by using the LED on the switchboard, if any. |
If the LED on the switchboard does not operate, check the LED and the voltage power supply. |
|
3 |
Remove the auxiliary terminal shield from a drawout device, if present. |
|
|
4 |
For a MasterPacT MTZ2/MTZ3 device, remove the terminal block identification plate. |
|
|
5 |
Identify and disconnect all wires for the CD, CT, and CE position contacts, and EF auxiliary contacts, if present. |
|
|
6 |
For MasterPacT MTZ1, use an ohmmeter or tester:
For MasterPacT MTZ2/MTZ3, use an ohmmeter or tester:
|
If a contact does not operate:
If the problem persists, contact your Schneider Electric Services representative. |
|
7 |
If the device has other CD contact blocks, check the corresponding contacts. |
|
|
8 |
Put the device in the test position. |
Checking Position Contacts With Device in Test Position
The CT position contacts indicate that the device is in the test position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the device is in the test position. NOTE: If
needed, refer to device racking operations as per procedure
Chassis NII_Z_1.
|
|
|
2 |
Check that the signal is consistent with the device position by using the LED on the switchboard, if any. |
If the LED on the switchboard does not operate, check the LED and the voltage power supply. |
|
3 |
For MasterPacT MTZ1, use an ohmmeter or tester:
For MasterPacT MTZ2/MTZ3, use an ohmmeter or tester:
|
If a contact does not operate:
If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
If the device has other CT contact blocks, check the corresponding contacts. |
|
|
5 |
Put the device in the connected position. |
Checking Position Contacts With Device in Connected Position
The CE position contacts indicate that the device is in the connected position.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the device is in the connected position. NOTE: If
needed, refer to device racking operations as per procedure
Chassis NII_Z_1.
|
|
|
2 |
Check that the signal is consistent with the device position by using the LED on the switchboard, if any. |
If the LED on the switchboard does not operate, check the LED and the voltage power supply. |
|
3 |
For MasterPacT MTZ1, use an ohmmeter or tester:
For MasterPacT MTZ2/MTZ3, use an ohmmeter or tester:
|
If a contact does not operate:
If the problem persists, contact your Schneider Electric Services representative. |
|
4 |
If the device has other CE contact blocks, check the corresponding contacts. |
|
|
5 |
Reconnect all the wires for the CD, CT, and CE position contacts. |
|
|
6 |
For MasterPacT MTZ2/MTZ3 with optional EF auxiliary contacts, check operation of these contacts. |
|
|
7 |
Put the terminal block identification plate and the auxiliary terminal shield back in place. |
Wiring Diagram of EF Auxiliary Contacts (Option on MasterPacT MTZ2/MTZ3)
The availability of the EF auxiliary contacts depends on the device.
Checking Operation of EF Auxiliary Contacts (MasterPacT MTZ2/MTZ3)
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Check that the device and the chassis are de-energized
on the upstream and downstream terminals.
Failure to follow these instructions will result in death or serious injury.
|
This EF information combines the device connected (CE) contact and device closed (OF) contact to produce the circuit connected/closed signal.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Put the device in the connected position. |
|
|
2 |
Close the device. |
|
|
3 |
Check that the signal is consistent with the device position by using the LED on the switchboard, if any. |
If the LED on the switchboard does not operate, check the LED and the voltage power supply. |
|
4 |
With the device in the connected position and with poles closed, use an ohmmeter or tester:
|
If a contact does not operate:
If the problem persists, contact your Schneider Electric Services representative. |
|
5 |
Open the device. |
|
|
6 |
With the device in the connected position and with poles open, use an ohmmeter or tester:
|
|
|
7 |
If the device has other EF auxiliary contact block, check them. |
|
|
8 |
Put the terminal block identification plate and the auxiliary terminal shield back in place. |
DANGER