Auxiliaries NIII_Z_2: Check Closing Operation with XF Closing Voltage Release at 0.85 Un
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check closing the device with the XF closing voltage release at 0.85 Un. |
|
Goal |
Verify that the device closes electrically at Umin. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
Connect the XF closing voltage release to an external power supply. |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Charged |
N/A |
|
Drawout |
Open |
Charged |
Removed from chassis |
XF Closing Voltage Release Wiring Diagram
Closing Procedure with the XF Closing Voltage Release
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK
When using the adjustable external power supply, take
all suitable measures to protect against electric shock.
Failure to follow these instructions will result in death or serious injury.
|
Before starting this check, it is advisable to execute a few electrical opening and closing cycles as per procedure Mechanism NII_Z_1.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Disconnect supply wires on the customer terminal block. |
|
|
2 |
Connect the adjustable external power supply and external pushbutton according to the corresponding wiring diagram above. |
|
|
3 |
Set the external power supply voltage to 0.85 Un (Un = customer auxiliary voltage). |
|
|
4 |
Press the external pushbutton to close the device. The device closes. |
If the device does not close:
If the problem persists, contact your Schneider Electric Services representative. |
|
5 |
Reconnect the customer terminal block according to the initial wiring. |
|
|
6 |
Check that the device electrically closes according to procedure Mechanism NII_Z_1. |
DANGER
DANGER