Mechanism NII_Z_3: Check the Complete Closing of Device Poles
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check that when the spring charging handle is pulled down with the device in the closed position and the mechanism charged, the device does not open. |
|
Goal |
Verify that the poles are closed and mechanically latched after closing the device manually. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
This check must be carried out manually. On fixed devices equipped with the MCH gear motor, disconnect the auxiliary circuit for the MCH gear motor (terminals B1 and B2). |
|
Necessary tools |
– |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected |
Checking Device Pole Complete Closing
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Manually charge the mechanism by pulling the spring charging handle down six times. |
|
|
2 |
Press the closing pushbutton to close the device. The device closes. |
If the device does not close, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
|
3 |
Pull the spring charging handle down. The device must remain closed. |
If the device opens (the indicator
shows Contact your Schneider Electric Services representative. |
DANGER