Mechanical Interlocking NII_Z_1: Operate Interlocking Systems
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the locking and unlocking of the interlocked devices. |
|
Goal |
Verify the operation of the interlocking system between interlocked devices. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
– |
|
Preliminary Conditions
The devices must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the devices.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Open |
Discharged |
N/A |
|
Drawout |
Open |
Discharged |
Test |
Checking the Locking and Unlocking of Interlocked Devices
Follow the procedure to check the locking and unlocking of the following interlocking systems:
-
Cable interlocking system:
-
Two sources
-
Three sources
-
Two sources and one replacement
-
Two sources and one coupling
-
Cable-type door interlock
-
-
Rod interlocking system
-
Electrical interlocking system
-
IVE electrical interlocking system
-
Custom electrical interlocking system
-
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Perform at least one manual operating sequence without power to check that the interlocking system operates correctly in all situations. Refer to the relevant instruction sheet for the interlocking system installed on the device. |
If an interlocking system is not operating correctly, contact your Schneider Electric Services representative. |
|
2 |
Lock the closing pushbuttons of all interlocked devices with padlocks sharing the same key. |
The VBP pushbutton locking accessory is mandatory to provide redundancy in addition to the mechanical interlocking system. Install a VBP pushbutton locking accessory on each interlocked device, if not already installed. Refer to the relevant instruction sheet for accessory installation. |
DANGER