Chassis Locking NII_Z_1: Operate Chassis Keylocking System
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check the locking and unlocking of the chassis with keylocks in the disconnected position or in any position, according to the chassis locking configuration. |
|
Goal |
Verify the chassis keylocking system with the optional VSPD chassis locking accessory correctly operates. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
Racking handle |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Disconnected |
Determining the Chassis Locking Configuration
The MasterPacT MTZ drawout devices offer two chassis locking possibilities with keylocks:
-
In the disconnected position.
-
In any position (disconnected, test, or connected).
To determine the chassis locking possibility, move the device to the connected or test position:
-
If you cannot pull out the padlocking tab, the chassis can be locked in the disconnected position only. Execute the locking procedure then the unlocking procedure.
-
If you can pull out the padlocking tab, the chassis can be locked in the disconnected, test, or connected position. The locking and unlocking procedures are the same as with chassis in the disconnected position. Execute these procedures in each position: connected, test, disconnected.
The following table shows the chassis locking configurations.
|
Chassis locking system |
Device position in the chassis |
Padlocking tab |
Racking handle insertion with chassis locked |
|---|---|---|---|
|
Chassis locking in the disconnected position |
Connected |
Cannot be pulled out |
Possible |
|
Test |
Cannot be pulled out |
Possible |
|
|
Disconnected |
Can be pulled out |
Not possible |
|
|
Chassis locking in any position |
Connected |
Can be pulled out |
Not possible |
|
Test |
Can be pulled out |
Not possible |
|
|
Disconnected |
Can be pulled out |
Not possible |
Checking Chassis Locking with Device in the Disconnected Position
For chassis with two keylocks, execute the following procedure for each keylock. Locking with one key is sufficient to lock racking operations.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
With the key captive in the keylock, check that the chassis is not locked. |
If the key is missing or broken, replace the keylock. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
2 |
Verify that the racking handle is not inserted in the racking handle socket. |
|
|
3 |
Turn the key counterclockwise, and then remove it. |
If the key does not turn, replace the keylock. |
|
4 |
Check that the racking handle cannot be inserted into the racking handle socket. |
If the racking handle can be inserted, check that the lock support is correctly installed (refer to MasterPacT MTZ - VSPD Disconnected Position Locking - Instruction Sheet). If the lock support is damaged, replace it. If the keylock is corroded, replace it. Then do the procedure again. If the problem persists, contact your Schneider Electric Services representative. |
|
5 |
Unlock the chassis and remove the key. Then do the procedure with the second key, if any. |
Checking Chassis Unlocking with Device in the Disconnected Position
Before starting this check, verify that the chassis is locked in the disconnected position.
For chassis with two keylocks, execute the following procedure for each keylock. Both keys must be inserted in the keylocks to unlock the chassis.
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Put the key in the lock. |
|
|
2 |
Turn the key clockwise and check that the key remains captive. |
If the key does not turn, replace the keylock. Refer to the MasterPacT MTZ with MicroLogic X Control Unit - Catalog for spare parts. |
|
3 |
Check that the racking handle can be inserted into the racking handle socket so that racking operations can be carried out. |
If the racking handle cannot be inserted, check that the lock support is correctly installed (refer to MasterPacT MTZ - VSPD Disconnected Position Locking - Instruction Sheet). If the lock support is damaged, replace it. If the keylock is corroded, replace it. Then do the procedure again. If the problem persists, contact your Schneider Electric Services representative. |
DANGER