Power Connections NIII_Z_1: Check Connection System
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify normal temperature rise on device and customer connections according to IEC standards. |
|
Frequency |
Refer to Recommended Frequency for the Intermediate End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
– |
– |
N/A |
|
Drawout |
– |
– |
Removed from chassis |
Example of Hardware Connection
Fixed Device: Checking Mounting of Connection Terminals to Device and Cables And/Or Busbars to Connection Terminals
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Disconnect busbars from all the connection terminals. Connection types: |
Advise customer in case of damage to busbars noticed during disconnection. |
|
2 |
Check the recommended torque value on the device: |
|
|
3 |
Make sure that the screws are not overtightened: |
If a screw cannot be tightened to this value, contact your Schneider Electric Services representative. |
|
4 |
Clean the busbar contact surfaces and customer terminals by using a white abrasive pad. |
If there is a major change in color, contact your Schneider Electric Services representative. |
|
5 |
Disconnect cables from all the connection terminals. |
Advise customer in case of damage to cables noticed during disconnection. |
|
6 |
Clean the contact surfaces of the cable lugs by using a white abrasive pad. |
Advise customer in case of damage to the cable insulation (for example, cracks or cable shrinkage). |
|
7 |
Reconnect the cables and/or busbars with a new set of bolts, nuts, and washers, and then tighten to the recommended torque. NOTE: Standard connection hardware
is class 8.8 steel hardware with contact washers. For MTZ2 40, MTZ3 40, MTZ3 50, and MTZ3 63, it is recommended
to use A80 stainless steel hardware.
|
Drawout Device: Checking Mounting of Connection Terminals to Device and Cables And/Or Busbars to Connection Terminals
Terminal Mounting on Device and Recommended Tightening Torque
Refer to the following documentation:
-
MasterPacT MTZ1 - Connectors - Instruction Sheet
-
MasterPacT MTZ2/MTZ3 - Connectors - Instruction Sheet
Recommended Tightening Torque of Connecting Busbars
The following table shows the tightening torques to be used for connecting busbars (Cu ETP - French standard NFA 51-100) to the circuit breaker. These values are for use with copper busbars and steel nuts and bolts, class 8.8. The same torques can be used with AGS-T52 quality aluminum bars (French standard NFA 02-104 or American National Standard H-35-1).

|
Ø (mm) Nominal |
Ø (mm) Drilling |
Tightening torques (N•m) with grower or flat washers |
Tightening torques (N•m) with contact or corrugated washers |
|---|---|---|---|
|
10 |
11 |
37.5 |
50 |
DANGER
DANGER