Chassis NII_Z_3: Check EIFE Chassis Position Limit Switches
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
|
Procedure characteristics |
Description |
|---|---|
|
Action |
|
|
Goal |
Verify consistency between actual position of the device in the chassis and the indications given by the chassis position limit switches of the EIFE interface. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
– |
|
Necessary tools |
|
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
N/A |
N/A |
N/A |
|
Drawout |
Open |
Discharged |
Test |
Checking that the EIFE Interface Communicates Correctly
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
If the device is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
|
2 |
Connect a PC running EcoStruxure Power Commission software to one of the Ethernet communication ports on the EIFE interface by using a standard Ethernet cable. |
|
|
3 |
Launch EcoStruxure Power Commission software. |
|
|
4 |
Click . |
|
|
5 |
In the window, check that the IP address of the EIFE interface is indicated. |
If the IP address of the EIFE interface does not display:
|
|
6 |
Click . Result: The device that you want to communicate with appears in . |
|
|
7 |
Select the device and click . |
|
|
8 |
In the window, click (green button). |
|
|
9 |
Click the section. Result: The product switchboard displays. |
|
|
10 |
In the tab, check that is . |
If the device position is not correctly displayed in EcoStruxure Power Commission software, follow the procedure to check manually the operation of the chassis position limit switches of the EIFE interface. |
|
11 |
Rack in the device to the connected position. |
|
|
12 |
Check that is . |
|
|
13 |
Rack out the device to the disconnected position. Result: A message is displayed: . |
|
|
14 |
Click to acknowledge the message. |
|
|
15 |
Click the tab. |
|
|
16 |
Rack in the device to the test position. |
|
|
17 |
In check that increments. |
If the counters do not increment correctly in EcoStruxure Power Commission software, replace the EIFE interface and do the procedure again. |
|
18 |
Rack in the device to the connected position. |
|
|
19 |
In check that increments and in check that the date and time are correct. |
If the counters do not increment correctly in EcoStruxure Power Commission software, replace the EIFE interface and do the procedure again. |
Manually Checking Operation of EIFE Chassis Position Limit Switches
If the chassis position is not correctly indicated in EcoStruxure Power Commission software, check the operation of the chassis position limit switches manually, by following the three stages described below:
| Stage | Description |
| 1 |
Remove the EIFE interface. |
| 2 |
Check the limit switches by operating them manually. |
| 3 |
Reinstall the EIFE interface. |
Follow this procedure to remove the EIFE interface:
|
Step |
Action |
|---|---|
|
1 |
Remove the auxiliary terminal shield. |
|
2 |
Remove the Ethernet cable (A) from the EIFE interface. |
|
3 |
Disconnect the ULP port module cord from the ULP port module and the EIFE interface (B). |
|
4 |
Remove the terminal block identification plate. |
|
5 |
Remove the EIFE interface by using a thin screwdriver inserted into the slot in the metal plate at the top of the EIFE interface, and releasing the clips holding the top of the EIFE interface in place. |
|
6 |
Remove the screwdriver and press down on the EIFE interface to unclip the bottom clips and pull out the EIFE interface. |
|
7 |
Reconnect the Ethernet cables to the EIFE interface to perform the test. |
Follow this procedure to check the actuators and operation of the EIFE chassis position limit switches:
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
Check that the actuators move freely. |
If the actuators do not operate correctly:
|
|
2 |
Locate the three limit switches on the back of the EIFE interface. |
|
|
3 |
When no limit switch is pressed, check that in EcoStruxure Power Commission software is . |
|
|
4 |
Press and hold the two outside limit switches. |
|
|
5 |
Check that in EcoStruxure Power Commission software changes to . |
|
|
6 |
Press and hold the two limit switches on the right. |
|
|
7 |
Check that in EcoStruxure Power Commission software changes to . |
|
|
8 |
Exit EcoStruxure Power Commission software. |
Follow this procedure to reinstall the EIFE interface:
|
Step |
Action |
|---|---|
|
1 |
Remove the Ethernet cables from the EIFE interface. |
|
2 |
Reinstall the EIFE interface. Refer to Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - Instruction Sheet. |
|
3 |
Reinstall the terminal block identification plate. |
|
4 |
Reconnect the Ethernet cables and ULP cord to the EIFE interface. |
|
5 |
Reconnect the ULP cord to the ULP port module. |
|
6 |
Reinstall the auxiliary terminal shield. |
|
7 |
Close the equipment door. |
|
8 |
Continue the procedure to check the operation of the EIFE interface from step 15. |
DANGER