Control Unit NII_Z_2: Check Ground-Fault (MicroLogic 6.0 X) or Earth-Leakage (MicroLogic 7.0 X) Protection Function
Safety Instructions
DANGER |
|---|
|
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
Procedure Definition
This procedure is valid for circuit breakers equipped with a MicroLogic 6.0 X or MicroLogic 7.0 X control unit.
|
Procedure characteristics |
Description |
|---|---|
|
Action |
Check that the device trips on ground-fault (MicroLogic 6.0 X) or earth-leakage (MicroLogic 7.0 X) by using the test button on the control unit. |
|
Goal |
Verify that the ground-fault or earth-leakage protection functions operate. |
|
Frequency |
Refer to Recommended Frequency for the Routine End-User Maintenance Program. |
|
Special indications |
Connect the MicroLogic X control unit to a power supply. For example, connect the Mobile Power Pack external battery to the MicroLogic USB port. |
|
Necessary tools |
– |
|
Preliminary Conditions
The device must comply with the conditions specified below. Refer to the MasterPacT MTZ User Guides to find instructions for operating the device.
|
Device installation type |
Position of poles |
Mechanism |
Device position in the chassis |
|---|---|---|---|
|
Fixed |
Closed |
Discharged |
N/A |
|
Drawout |
Closed |
Discharged |
Test |
Checking MicroLogic X Control Unit Trip Cause LED
|
Step |
Action |
Corrective action |
|---|---|---|
|
1 |
If the device is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
|
2 |
To open the transparent cover, pull its upper right-hand side corner. |
|
|
3 |
Use a thin screwdriver to briefly push-in (<1 s) the test button, and then check that the Ig/IΔn LED is on and the screen display turns to red with the corresponding message. |
If the Ig/IΔn LED does not light up, contact your Schneider Electric Services representative. |
|
4 |
Check that the device trips and that the blue fault-trip reset button on the front cover pops out. |
|
|
5 |
Press and hold the Test/Reset button for 3 seconds to reset the trip cause LEDs. |
|
|
6 |
Manually charge the mechanism by pulling the spring charging handle down six times. When the spring charging handle no longer resists, the mechanism is charged. |
|
|
7 |
If the device is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
|
8 |
Press the closing pushbutton. The device must not close. |
If the device closes, check with customer order form:
|
|
9 |
Press the blue fault-trip reset button on the front cover to reset. |
If the blue fault-trip reset button does not reset, contact your Schneider Electric Services representative. |
|
10 |
Press the closing pushbutton. The device closes. |
If the device does not close, refer to troubleshooting in the appendix. If the problem persists, contact your Schneider Electric Services representative. |
DANGER